This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28075: Problem with ePWM X-BAR

Part Number: TMS320F28075

Tool/software: Code Composer Studio

Hello, I am Jongwoo Kim, and I am struggling with ePWM X-BAR.

My purpose is to produce DCAEVT1.sync signal from CMPSS.CTRIPH so that an ePWM module can be synchronized with the rising edge of the comparator output.

I tested 3 ways to achieve this function as follows:

1. CMPSS.CTRIPOUTH -> GPIO_OUT ------ wired connection ----> GPIO_in -> EXTSYNCIN -> synchronized.

2. CMPSS.CTRIPOUTH -> GPIO_OUT ------ wired connection ----> GPIO_in -> GPIO X-BAR -> TRIPx -> DCAH -> DCAEVT1.sync -> synchronized.

3. CMPSS.CTRPH -> ePWM X-BAR -> TRIPx -> DCAH -> DCAEVT1 .sync -> synchronized.

I successfully got the synchronized ePWM by using the methods 1 and 2. Therefore, I think there is no problem in CMPSS and DC module.

However, when I tried the method 3 (this is the most attractive way since it does not use the connection outside), ePWM module is not synchronized. just free running.

Therefore, I think the CMPSS.CTRPH -> ePWM X-BAR -> TRIPx steps in the method 3 has a problem.

In this case, could you give me some help? The followings are my settings for CMPSS and ePWM module. (please note that the comparator output and DC submodule are fine as I mentioned before)

(Comparator output is okay. CTRIPOUTH is also okay. But I am not sure CTRIPH is okay.)

Cmpss2Regs.COMPCTL.bit.CTRIPHSEL = 2;  // Digital filtered comparator output is uploaded to ePWM X-BAR

EPwmXbarRegs.TRIP10MUX0TO15CFG.bit.MUX2 = 1; // CMPSS2.CTRIPH -> MUX2 output -> TRIP10MUXENABLE switch

EPwmXbarRegs.TRIP10MUXENABLE.bit.MUX2 = 1; // TRIP10MUXENABLE enables MUX2

EPwmXbarRegs.TRIPOUTINV.bit.TRIP10 = 0; // Active high

EPwm7Regs.DCTRIPSEL.bit.DCAHCOMPSEL = 9; // TRIPIN10 is selected for DCAH

(I also tested DC submodule so that DCAH->DCAEVT1.sync is working.)

Thank you for your interest in advance.

Sincerely,