Tool/software: Starterware
Hi Folks,
I've been having a little play with the instaspin identify primarily as part of the instaspin-FOC lab2b. When I run the lab I can get a motor spinning and change velocity etc, but I noticed that when I repeat the identify process i get wildly varying Lsq vals. They range from 4.98x10^-10 to 0.0038. This doesn't seem quite right to me, especially given that the winding resistance comes out at a constant 13ohms.
I do have some motor data and the terminal resistance and terminal inductance for the motor in question but I am uncertain if this is of any use in this situation as the terminal resistance does not seem to match the value measured by the identify process. The vals being R = 2.8ohm, and L = 0.92mH.
Little bit puzzled, could anybody suggest why this might be?
Thanks