Part Number: TMS320F28335
Tool/software: Code Composer Studio
Is there a way to unlock the CSM (code security module) while "jump to flash" boot mode is enabled for the F28335?
I am using a XDS100 v2.
I tried using the solution here: https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/493016
to enable "wait-in-reset", but it still does not allow me to connect to the debugger.
It just keeps providing "Error -1135 @ 0x0", since I guess it immediately locks out the JTAG immediately after boot.
When I use "branch to check boot mode", it can unlock fine. However, I would rather not have to do anything with the hardware.
It can't seem to "halt the target on a connect" when it can't even begin connecting.