This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027F: locked or not connected

Part Number: TMS320F28027F
Other Parts Discussed in Thread: UNIFLASH

Hi all,

I'm working with TMS320F28027F.

The hardware was working fine. I made a lot of testing and debugging, so it is not a hardware design issue.

I started to load a program to flash using CCS and suddenly was not able to do so. The error was

C28xx: Flash Programmer: Device is locked or not connected. Operation cancelled.
C28xx: File Loader: Memory write failed: Unknown error

I did not play with locking password keys and the hardware is OK.

I also tried Uniflash tool. I can connect to the device and I can read the flash memory, hence I am sure the device is not locked and is connected.

What else could go wrong?

Thank you a lot in advance.