Other Parts Discussed in Thread: C2000WARE
Hi all,
I'm starting to work on coding for an interleaved converter with four phases switching at 400kHz per leg. Because of the 100MHz EPWMCLK limitation I need to setup a fractional phase offset, but I also need to be able to use the CMPAHR and CMPBHR functionality to get acceptable resolution to control of the output voltage. Is there any way to be able to use a fixed setting for the TBPHSHR register to get a fixed fractional phase shift while using the HRPWM module CMPAHR and CMPBHR registers to control the actual pulse widths?
I end up with a phase offset of 62.5 counts for one of the phases, and 187.5 for another, while the other only needs an integer offset of 125 counts.