Other Parts Discussed in Thread: ADS6125
I require 3 SPIs and SPI A and SPI B are available but GPIO 70 is wired to the CAN transceiver U3 thus the SPI C is not available. Is it possible to configue SPI C via GPIOs if the CAN is not used?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I require 3 SPIs and SPI A and SPI B are available but GPIO 70 is wired to the CAN transceiver U3 thus the SPI C is not available. Is it possible to configue SPI C via GPIOs if the CAN is not used?
Hi Jingtai,
If you need to use SPI-C, I'd recommend depopulating R43 and R44. You can then utilize GPIO69, GPIO71 and GPIO72 via the LaunchPad header without fear of contention.
If you need a SPISOMIC signal, you'd then need to solder a wire onto the resistor pad of R44 in order to gain access to GPIO70.
Hopefully this helps!
Thank you,
Brett
Hi,
Jingtai said:If the CAN interface is not connected the R43 and R44 will not work and they will be kept there. Is it ok?