This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: Interfacing MATLAB (with TI Add On) with TI C2000 Hardware Kit

Part Number: TMS320F28035
Other Parts Discussed in Thread: CONTROLSUITE
Dear Sir,
Kindly refer to the attachment of the error, while trying to build the example model - TMDSHVMTRPFCKIT + F28035 Piccolo: c28035pmsmfochvkit_ert.slx
Hoping for a positive response.
Thanks & Regards
Reshma Ravi
  • Hi Reshma,

    Please post on Matlab forum for Matlab related errors and support.

    Regards,
    Gautam
  • Hi,
    We are able to build and flash the model after reinstalling TI Add on package and installing BIOS for CCS.
    When the model is chosen to be in 'Position sensing using Hall Sensors', the program is flashed to the target, but the motor does not run. The model used is an example model provided in mathworks website titled "Permanent Magnet Synchronous Motor Field-Oriented Control". We have chosen 'TMDSHVMTRPFCKIT + F28035 Piccolo: c28035pmsmfochvkit_ert.slx' as the available version of this example.
    Kindly guide to monitor and control the motor parameters from host computer (serial data transfer).

    Hoping for a positive response.
    Best Regards
    Reshma Ravi
  • Did you go through these documents: C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v2.1\~Docs
  • Hi,

    In order to monitor and control the motor parameters from host computer (serial data transfer), please refer the example  c2000_host_read.slx for a model on Host side that receives the serial data. And please refer example model c28027pmsmfoc_ert.slx for an example on how to send the serial data from target.

    You may want to contact the MathWorks Tech Support for more information.

    Regards,

    Venkatesh C