Part Number: DRV8301-69M-KIT
Other Parts Discussed in Thread: DRV8301, BOOSTXL-DRV8301, LAUNCHXL-F28027F
Hello,
I would like to design my own schematic of the DRV8301-69M/F kit.
I have already got the kit however I would like create a bare minimum board of it.
I will essentially only use a pot, 2 buttons and few LEDs.
The app is really simple. Start and Stop with speed control with the pot.
Therefore, I will not be using SPI,CAN, QEP/CAP etc.
So, I need to double check with the experts out there,
1-Do I need to populate the following?
U2,U3,U4 - voltage reg and CAN
U5 - SPİ
U7 - QEP/CAP
2-Other components that I can remove?
Many thanks
Nobel