Part Number: INSTASPINUNIVERSALGUI
Other Parts Discussed in Thread: DRV8301
Tool/software: Code Composer Studio
Hello,
I would ask a question about ADC full scale current setting of InstaSpin lab.
On InstaSpin lab, "USER_ADC_FULL_SCALE_CURRENT_A" value on user.h is 33.0A ( Not equal to "16.5A"), with boostxldrv8301_revB kit.
I think the calculation is 3.3(V) / ( 0.01 ohm ( current sence resistance) * 10 (Drv8301 amplifier gain) ) , and the definition is
relevant to the 1LSB of A/D conversion on MCU.
Is it correct ?
Hiroyasu