Part Number: LAUNCHXL-F28377S
Hi everybody,
I have a question about the Moduls of communication. I want to try a fast communication between Master and 1 or 2 Slaves. So I searched in datasheet how fast each communication-Modul is. Because i couldn´t find a answer, i would ask the TI community.
How fast are the following communications:
SPI
SCI
McBSP
uPP
...
Since yet, I tried SPI and McBSP. But in SPI i only could do a 20 MHz Baudrate. In Datasheet stays "max. 50MHz in High Speed Mode". But i couldn´t reach this value, althought i set HS_MODE to 1.
McBSP had problems with higher Baudrates than 3,125 MHz. (SYSCLK (200 MHz) / LSPCLKDIV (4) and /CLKGDV (16) = 3,125MHz)
For this tests I connected a Master F28377s Launchpad with a Slave F28377s Launchpad.
I hope someone can write something about "Where I find the max. speed" and maybe about "how much Baudrate is OK for communication and which isn´t good or impossible".
Thanks!
Best wishes
Stefan