Part Number: F28M35M52C
i have 10 boards that contain concerto and tiva.
i used up to now the XF28M35h52 and the LX4F232H and all board were working.
i upgraded the boards to F28M35h52 and TMC123G .
5 boards are working fine and 5 boards faulty
on the faulty boards a periodic reset pulses exist on the common reset line
it is impossible to program both u controllers
the u controllers are using the same jtag chain
GPIO 35,34,43,47 are puled up via 10k resistors
EM0,EM1 puled up via 4.7k resistors
please your advice
Tsfania