I hope I am posting this in the right place to get an answer.
I am working on the TI Renewable Energy kit. I want to measure the current at the input of the boost converter, but I am getting vague values.
Could anyone help me with this?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I hope I am posting this in the right place to get an answer.
I am working on the TI Renewable Energy kit. I want to measure the current at the input of the boost converter, but I am getting vague values.
Could anyone help me with this?
Thanks!
Please check the schematic and see what the documentation says about this measurement. Which current are you referring to? Not sure about the latest version of the software and the board but I believe all currents and voltages can be measured.
Hi
Yes, I got it. It works perfectly fine. You just have to map input current like its done for battery charging current. Here, you also have to adjust the offset values.
Hope this helps.
Hi,
Thank you for your reply. I have managed to do it. However, the input current measurement has a lot of noise (0.05-0.1A). Do you have that noise?
OK.
Anyone else has noise in the current measurements (both input and battery currents)? I am working with a small input input current (between 0 and 0.5 A) and the measurements I am getting oscillate a lot (0.05-0.1 A) even if the input current is constant. Is this normal?
Thank you!