This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8312-69M-KIT: AC adapter of this KIT and 'DRV8312-C2-KIT'

Part Number: DRV8312-69M-KIT

Dear all,

Could you teach about AC adapter spec of these two KITs?

I could not see adapter spec because there are server error.

I must choose AC adapter of Japan certificated.

Please teach these adapter specs I should use.

 Best regards,

  • The kit package provides 3 different adapter plug which can support Europe, US and UK, the input in 100~240V/50-60Hz/1.5A. It should be used in Japan.
  • Hi Yanming-san,

    Thank you for your reply.
    I understand that this adapters will work in Japan, but we can not provide this adapter with my customer because this adapter don't have Japan certification (PSE certification).
    Therefore, I have to buy same spec adapter for this kit in Japan.

    Could you teach me about the output voltage and the form of plug?
    Or could you teach me about the product number of plug?

    Best regards,