Part Number: TMS320F28035
Other Parts Discussed in Thread: TMDSDOCK28035, CONTROLSUITE
Hi,
I am using SIM900 Module to communicate with Piccolo 28035 Micro controller.
I have to do the follwoing things:
1. Data to be sent from TX Buf of Microcontroller
2. AT Commands to be sent from TX Buf of Microcontroller along with delay.
Whatever I have sent, I have to see in RXBUF.
how to combine points 1&2 in the same code.
Can anyone help.