Part Number: TMS320F28379D
Tool/software: Code Composer Studio
I'm using TMS320F28379D with Code Composer Studio.
'2837x_RFFT_ADC' project is used.
I want to take square root of data in 'RFFTmagBuff'. So, I built 'RFFTsqrtBuff' in 'main.c', and I think I have some mistake, but I cannot find it.
Please help me how to do it!
Here is my main.c code
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
#include "fpu_rfft.h" // Main include file
#include "math.h"
#include "examples_setup.h"
#include "F2837xD_device.h"
#define RFFT_STAGES 11 //9
#define RFFT_SIZE (1 << RFFT_STAGES)
#define F_PER_SAMPLE (ADC_SAMPLING_FREQ/(float)RFFT_SIZE)
#pragma DATA_SECTION(RFFTin1Buff,"RFFTdata1")
uint16_t RFFTin1Buff[2*RFFT_SIZE];
#pragma DATA_SECTION(RFFTmagBuff,"RFFTdata2")
float RFFTmagBuff[RFFT_SIZE]; // /2+1
#pragma DATA_SECTION(RFFToutBuff,"RFFTdata3")
float RFFToutBuff[RFFT_SIZE];
#pragma DATA_SECTION(RFFTF32Coef,"RFFTdata4")
float RFFTF32Coef[RFFT_SIZE];
RFFT_ADC_F32_STRUCT rfft_adc;
RFFT_ADC_F32_STRUCT_Handle hnd_rfft_adc = &rfft_adc; // & Bit Operator
RFFT_F32_STRUCT rfft;
RFFT_F32_STRUCT_Handle hnd_rfft = &rfft;
volatile uint16_t flagInputReady = 0;
volatile uint16_t sampleIndex = 0;
uint16_t pass = 0;
uint16_t fail = 0;
__interrupt void adcaIsr();
int16_t main(void)
{ // Locals
uint16_t i, j;
float freq = 0.0;
float freq1 = 0.0;
float RFFTsqrtBuff[RFFT_SIZE];
#ifdef FLASH
EALLOW;
Flash0EccRegs.ECC_ENABLE.bit.ENABLE = 0;
memcpy((uint32_t *)&RamfuncsRunStart, (uint32_t *)&RamfuncsLoadStart, (uint32_t)&RamfuncsLoadSize );
FPU_initFlash();
#endif // FLASH
FPU_initSystemClocks();
FPU_initEpie(); // Setup ADC-A
FPU_initADCA();
FPU_initEPWM(); // Setup EPWM1A as the sampling clock, EPWM2A as the signal to be sampled
EALLOW; // Map ISR functions
PieVectTable.ADCA1_INT = &adcaIsr; // Function for ADCA interrupt 1
EDIS; // Enable Global Interrupts and Higher Priority Real-Time Debug Events:
PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable ADC1INT
IER |= M_INT1; // Enable group 1 interrupts
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global real time interrupt DBGM
FPU_startEPWM(); // Start up the EPWMs
hnd_rfft_adc->Tail = &(hnd_rfft->OutBuf);
hnd_rfft->FFTSize = RFFT_SIZE; // FFT size
hnd_rfft->FFTStages = RFFT_STAGES; // FFT stages
hnd_rfft_adc->InBuf = &RFFTin1Buff[0]; // Input buffer (16-bit ADC) input
hnd_rfft->OutBuf = &RFFToutBuff[0]; // Output buffer
hnd_rfft->CosSinBuf = &RFFTF32Coef[0]; // Twiddle factor
hnd_rfft->MagBuf = &RFFTmagBuff[0]; // Magnitude Output Buffer
RFFT_f32_sincostable(hnd_rfft); // Calculate Twiddle Factor
for (i=0; i < RFFT_SIZE; i++){
RFFToutBuff[i] = 0; // Clean up Output Buffer
}
for (i=0; i < RFFT_SIZE; i++){ // /2
RFFTmagBuff[i] = 0; // Clean up Magnitude Buffer
}
for (i=0; i < RFFT_SIZE; i++){ // /2
RFFTsqrtBuff[i] = 0; // Clean up Square-Root Buffer
}
while(1){
while(flagInputReady == 0){}; // Wait on ADC ISR to set the flag before proceeding
RFFT_adc_f32(hnd_rfft_adc); // Calculate real FFT with 16-bit ADC input
flagInputReady = 0; // Reset the flag
RFFT_f32_mag(hnd_rfft); // Calculate magnitude
j = 1;
freq = RFFTmagBuff[1];
freq1 = RFFTsqrtBuff[1];
for(i=2;i<RFFT_SIZE;i++){ // /2+1
if(RFFTmagBuff[i] > freq){
j = i;
freq = RFFTmagBuff[i];
}
for(i=2;i<RFFT_SIZE;i++){
if(RFFTsqrtBuff[i] < freq1){
j = i;
freq1 = sqrtf(RFFTmagBuff[i]);
}
}
}
freq = F_PER_SAMPLE * (float)j;
freq1 = F_PER_SAMPLE * (float)j;
}
done();
return 1;
}
__interrupt void adcaIsr()
{
RFFTin1Buff[sampleIndex++] = AdcaResultRegs.ADCRESULT0;
if(sampleIndex == (2*RFFT_SIZE - 1) ){
sampleIndex = 0;
flagInputReady = 1;
}
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; // Clear INT1 flag
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------