Hello
I have problem regarding configuration PWM10 and PWM11 on LaunchPad_F28377S to generate signals.
Based on example epwm_up_aq_cpu01.c I can configure PWM 4,6,8 but I can't do this for PWM 10,11.
Bellow my code. Maybe somebody help me with this issue. I sent a lot of time to solve it.
Best Regards
Dariusz
#include "F28x_Project.h"
#include "F2837xS_Examples.h"
CpuSysRegs.PCLKCR2.bit.EPWM10=1; // enable PWM10
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO18 = 1; // Disable pull-up on GPIO18 (EPWM10A)
GpioCtrlRegs.GPAPUD.bit.GPIO19 = 1; // Disable pull-up on GPIO19 (EPWM10B)
GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 1; // Configure GPIO2 as EPWM10A
GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 1; // Configure GPIO3 as EPWM10B
EDIS;
EPwm10Regs.TBPRD = 3125; // Set timer period
EPwm10Regs.TBPHS.bit.TBPHS = 0x0000; // Phase is 0
EPwm10Regs.TBCTR = 0x0000; // Clear counter
EPwm10Regs.TBCTL.bit.CTRMODE = 2; // Count up-down
EPwm10Regs.TBCTL.bit.PHSEN = 0; // Disable phase loading
EPwm10Regs.TBCTL.bit.HSPCLKDIV = TB_DIV2; // Clock ratio to SYSCLKOUT
EPwm10Regs.TBCTL.bit.CLKDIV = TB_DIV2; // Slow just to observe on
EPwm10Regs.CMPA.bit.CMPA =1562;
EPwm10Regs.CMPB.bit.CMPB =1562;
EPwm10Regs.AQCTLA.bit.CAU = 2; // Set PWM2A on Zero
EPwm10Regs.AQCTLA.bit.CAD = 1;
EPwm10Regs.AQCTLB.bit.CAU = 2; // Set PWM2B on Zero
EPwm10Regs.AQCTLB.bit.CAD = 1;
EPwm10Regs.DBCTL.bit.OUT_MODE = 3;
EPwm10Regs.DBCTL.bit.POLSEL = 1;
EPwm10Regs.DBCTL.bit.IN_MODE = 0;
EPwm10Regs.DBRED.bit.DBRED = 50;
EPwm10Regs.DBFED.bit.DBFED = 50;