Other Parts Discussed in Thread: SPRC097
We are having problem that the eva registers in the F2812 processor are
not getting loaded with the values which we gave in the program.
FOR
EXAMPLE:
MOV @T1CON,#9046h
after executing this
instruction we checked the memory mapping and T1CON is not taking the
value and the memory space allocated for the register is 0 itself.In the
DEASSEMBLY in place of the above instruction it is written as MOV
@1,#9046h.in the memory map the value is loaded in the 0x000001.
we
dont know how to correct it and if it is a error in the cmd file.PLEASE
HELP US URGENTLY...
PLZ HELP....URGENTLY
NEEDED.
Complete program including header files,build
options,cmd files,library files, interrupt files and all additional
files to be created in CCS 3.1 for generating pwm signal using F2812 DSP
processor in asm framework.It uses 6 step commutation and has feedback
through adc to change duty cycle.BLDC motor is a sensored (hall sensor)
motor. Duty cycle is varied according to the interrupt.
PLZ MAIL ME
THE PROGRAM BCOZ THIS IS OUR MAIN PROJECT AND OUR SLOT TIME PERIOD IS
GETTING OVER THIS MONTH..MY EMAIL ID IS
jr_anand@yahoo.com,san24dhu@gmail.com.