Other Parts Discussed in Thread: C2000WARE, CONTROLSUITE
Hi,
I need to use a timer in order to wakeup (interrupt) some function every constant period.
I checked example code in C2000ware but appropriate example is not there.
I try to code as follows;
1. initialize timer-0 in initialize function
2. set period time for timer-0 in initialize or other function
3. register the timer-0 and vector number and function which makes the interrupt every constant period
Are above sequence in code is correct, and do you know better example code?
Best Regards,
Takano