This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/DRV8701EVM: Example GUI Composer program is stuck on Loading Application

Part Number: DRV8701EVM

Tool/software: Code Composer Studio

I followed the instructions in the DRV8701EVM user's guide (SLVUAG3) and downloaded and installed the GUI Composer runtime. I then put the DRV8701EVM_GUIv1.0 in the ti/guicomposer/webapps folder and ran the DRV8701EVM_GUIv1.0.exe in that folder. The window opens and Loading Application... comes up with a loading bar and thats it. It hangs there forever. 

The same thing happens with the example modem_m3 application as well. 

I'm on a windows 7 machine.