Other Parts Discussed in Thread: CONTROLSUITE
Hello
Im working on a Project wich needs to be loaded Standalone from Flash and I have to save data to Flash. Based on SPRA958L I implemented the functionality to copy my Programm Code, the .econst and the .switch Symbols to Ram at Startup. I used SPRAB60 to implement a EEPROM Emulation in one Flash Sector and I used the 2806x_BootROM_API_TABLE_Symbols_fpu32.lib
If I programm the Device with CCS it works fine. My Code operates as it should and I'm able to write to Flash. If I reset the Device and let it boot from Flash the code works also but I'm not able to write to flash.I have figured out, that the Flash_Program Function of the API gets called but Returns a Error Code 30 which means Program Fail.
I'm wondering why it works when loaded from CCS but not from Flash. I've attached my linker cmd File below. Is there something different in the initilization when booted from Flash?
Thank You and best Regards
Andri
MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */
RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */
IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAML1 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
RAML2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
RAML4 : origin = 0x00A000, length = 0x002000 /* on-chip RAM block L4 */
RAML5 : origin = 0x00C000, length = 0x002000 /* on-chip RAM block L5 */
RAML6 : origin = 0x00E000, length = 0x002000 /* on-chip RAM block L6 */
RAML7 : origin = 0x010000, length = 0x002000 /* on-chip RAM block L7 */
RAML8 : origin = 0x012000, length = 0x002000 /* on-chip RAM block L8 */
USB_RAM : origin = 0x040000, length = 0x000800 /* USB RAM */
FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */
FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */
}
/* Allocate sections to memory blocks.
Note:
codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
execution when booting to flash
ramfuncs user defined section to store functions that will be copied from Flash into RAM
*/
SECTIONS
{
.cinit : > FLASHA, PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA, PAGE = 0
codestart : > BEGIN, PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = RAML3,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
LOAD_SIZE(_RamfuncsLoadSize),
PAGE = 0
csmpasswds : > CSM_PWL_P0, PAGE = 0
csm_rsvd : > CSM_RSVD, PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM1, PAGE = 1
.ebss : > RAML4, PAGE = 1
.esysmem : > RAML2, PAGE = 1
/* Initalized sections to go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : LOAD = FLASHB,
RUN = RAML6,
LOAD_START(_EconstLoadStart),
RUN_START(_EconstRunStart),
LOAD_SIZE(_EconstLoadSize),
PAGE = 1
.switch : LOAD = FLASHA,
RUN = RAMM0,
LOAD_START(_SwitchLoadStart),
RUN_START(_SwitchRunStart),
LOAD_SIZE(_SwitchLoadSize),
PAGE = 0
/* Allocate Memory for Register Map: */
.register : > RAML1, PAGE = 1
/* Allocate IQ math areas: */
IQmath : > FLASHA, PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
/* Allocate FPU math areas: */
FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD
/* Uncomment the section below if calling the IQNexp() or IQexp()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
*/
/* Uncomment the section below if calling the IQNasin() or IQasin()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
}
*/
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS, PAGE = 0, TYPE = DSECT
}