Part Number: TMS320F28075
Other Parts Discussed in Thread: OPA320, OPA350
Hey guys,
I'm working on a project with the TMS320F28075 and i got a few questions about the inner structure of the ADCs.
The datasheet of the F28075 describes that the PTP version has 19 pinouts for the ADC:
ADCIN14 & ADCIN15
ADCINA0 - ADCINA5
ADCINB0 - ADCINB5
ADCIND0 - ADCIND4
So the F28075 has a amount of 3 Independent ADCs with a 16 channel multiplexer. But i don't unterstand why every ADC has got a 16 channel multiplexer.
For example ADC A:
-ADCIN14 & ADCIN15 are connected to every ADC module
-ADCINA0 - ADCINA5
This is a sum of 8 channel which can be multiplexed to the ADC A, right? Is my comprehension about the ADC module right or wrong?
I have to convert 16 different analog signals, which pins should i use for it?
Kind regards,
Tom