Part Number: TMS320F28335
Other Parts Discussed in Thread: LM70
What are the proper hardware connections from the 28335 and the LM70 temperature sensor? Can the MISO/MOSI be tied directly together on the 28335, or should I add a 10K resistor on the MISO and then tie them together after? I assume the LM70 has a high impedance on the SI/O line, however isn't stated in the data sheet. My only concern with the 10K resistor is voltage drop.