This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSPLCKITV4-CEN: PLC application - PRIME mode.

Part Number: TMDSPLCKITV4-CEN


hi all:

I would like to establish a power line PRIME network with base node and service node.

By using prime_ hostappemu.exe, TMDSPLCKITV4 module seems to start searching base node and shows...

[15:21:59]:Attempting Stage 1 Connection to Base Node, attempt #1...
[15:21:59]:ECA_AppEmu_SETUP_ALARM_Handler: SET_ALARM returned success.
[15:21:59]:Attempting Stage 2 Connection to Base Node, attempt #1...
[15:21:59]:ECA_AppEmu_Connect_LLC: ATTACH to 00:00:00:00:00:00

How can I get a base node to connect to it? Is there anther app to set TMDSPLCKITV4 to be a base node?

Thank you very much.