This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377D: CLA processing threshold..

Part Number: TMS320F28377D


Tool/software: Code Composer Studio

Hi,

Is there a limit on the number of operations you can perform in a CLA subsystem? For example is it possible to implement the whole logic to generate a 3 phase waveform which contains 4 multiplications, 3 addition, 1 or 2 trigonometric conversions, 1 division, and a few logical operations, which are to be executed at each step. Even after following the procedures as above I am still getting error stating one or two variables are undefined(same as the error I got in the beginning). Any ideas?

Regards,

Venkatesh C