Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: BOOSTXL-DRV8301, CONTROLSUITE, C2000WARE,
Tool/software: Code Composer Studio
I'm working through tutorials. Actually, I'm trying to find one that works. My LaunchPad has a BOOSTXL-DRV8301 plugged into it, which supplies the power.
The build of Example_F2806xLaunchPad fails with the error below.
What's going on? I assume this project is a tutorial/educational, If so, I'm surprised that it doesn't build. How can I fix this?
Or is there a better starting place for newbies? (FYI, Example_F2802xLEDBlink doesn't seem to blink anything on the F28069M.)
Be careful with advice: I'm just starting out, so you can't assume I know very much about CCS.
>> Compilation failure
makefile:149: recipe for target 'Example_2806xLaunchPad.out' failed
warning: creating output section ".cio" without a SECTIONS specification
warning: creating ".esysmem" section with default size of 0x400; use the -heap
option to change the default size
"C:/ti/controlSUITE/device_support/f2806x/v140/F2806x_common/cmd/F28069.cmd", line 141: error:
program will not fit into available memory. run placement with
alignment/blocking fails for section ".ebss" size 0x223 page 1. Available
memory ranges:
RAML2 size: 0x400 unused: 0x0 max hole: 0x0
.ebss : > RAML2, PAGE = 1