Part Number: TMS320F28069M
Tool/software: Code Composer Studio
Hi,
I’m trying to calculate the instantaneous torque of a PMSM from the q-axis current and the rotor flux.
In the video “Teaching old motor new tricks”, which by the way is very helpful, it’s said that the torque=3/2*P/2*(lambda_dr*Iqs)
P:poles
Lambda_dr:rotor flux
In this post: e2e.ti.com/.../277190
David said “the motor torque can be calculated by simply multiplying the rotor flux linkage times the q-axis stator current times the number of rotor poles/2”.
I’m a little confused here.
The final goal is to compare experience (TI board) from simulation (Matlab).
From the Instaspin motion labs, the rotor flux is estimated to 0.103V/Hz:
But when I try to adjust settings of the PMSM Matlab model from my motor datasheet, it estimates the rotor linkage flux to 0.0174444 V.s:
Do you have detail of how Instaspin motion estimate the rotor flux linkage?
Thanks a lot!