This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Position Manager EnDat2.2 8/16MHz clock rate

Part Number: TMS320F28379D

I´m acutally working with TMS320F28379D on the Evaluation Board IDDK R2.2.1 and using Position Manager Software from the Control Suite. We would like to use the EnDat22 Library according to SPRUI35. In the documentation is the advice only to use 8MHz clock rate, but according to Heidenhain EnDat2.2 it is defined for up to 16MHz. Why is it not possible to use the 16MHz? Is there a limitation from the CLB or in the software library? Is a newer EnDat22 library available in futur wich could run 16MHz clock rate?