Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: TMS320F28379D
Hi,
I need to measure current from a LEM module. The output from the LEM is 0 ~ 5 V and I scaled it to 0 ~ 3 V by a voltage divider.
Now I am not quite sure about how to connect the LEM pins to the ADC pins of the MCU. I thought the connection should be in this way as follows. Does my connection look correct?
I heard that it is better to use Differential Input Model to reject the disturbance. However, I am not quite sure if it is possible to use Differential Input Model because the MCU and the LEM share the same ground in our case. Does anyone have any opinion or suggestion?
Thank you very much!
Sincerely,
Junfei Tang