Part Number: TMS320F28027F
Other Parts Discussed in Thread: DRV8301, MOTORWARE
Tool/software: Code Composer Studio
Hello all,
It's been a while since I'm trying to get to work with LAUNCHPAD TMS320F28027F + Booster pack DRV8301. The motor that I'm using it's the MAXON EC 22 partnumber: 386676 and I tried to verify the parameters with the GUI Composer universal as the normal workflow indicated by TI motorware solutions and running the Instaspin Labs compatible with my target device. After some modifications on user.h as below, the motor spin up as expected but even in lower speed, the motor housing heats above expected (126°C ~ 258.8F) and there isn't torque on its axis without any load present (free running). I tried to use the LAB10 with overmodulation and LAB5 speed PI controller and booth heat the motor despite spin the motor in the correct speed that I want ~ 28.200 kRPM. In attach follows the user.h with my modifications. Ps.: In the identification setup, the values read by the target were very similar to the motor sheets, but the temperature/torque issues are still present.