Part Number: LAUNCHXL-F28377S
Other Parts Discussed in Thread: DAC8560, TMS320F28377S, CONTROLSUITE
Hello TI community,
I am currently trying to communicate to the DAC8560 (http://www.ti.com/lit/ds/symlink/dac8560.pdf with my TMS320F28377S via SPI. The problem I am having is that the F28377S SPI shift register is 16 bits while the shift register on the DAC8560 is 24 bits. On page 20 of the DAC8560 data sheet is has two clauses that I think will cause be trouble. The first piece of information is that the chip-select signal must be brought high before each new write sequence. I am assuming this means I can only write 24-bits of data at a time before having to bring the chip-select line high. The second piece of information is that if the chip-select signal is brought high before the 24th falling edge, it acts as an interrupt to the write sequence. It then will reset the shift register and the write sequence will be seen as invalid; therefore, the DAC register will not be updated. The problem is that the TMS320F28377S says that each time it finishes sending it's maximum number of bits (in this case 16) it will bring the chip select signal high automatically. I was wondering if there is any way that I can get around this.