Part Number: TMS320F28377D
Other Parts Discussed in Thread: CONTROLSUITE
Hi,
We want to perfrom forward and inverse FFT of 256 sample real data(Array) using TMS320f28377D with library c28x_vcu2_library_fpu32.lib.
So we have been exploring controlsuite example project 2837x_vcu2_rfft_256.
Forward FFT is done using following steps:
// Step 1: Initialize CFFT object
CFFT.pInBuffer = buffer1Q15;
CFFT.pOutBuffer = buffer2Q15;
CFFT.init = (void (*)(void *))CFFT_init128Pt;
CFFT.run = (void (*)(void *))CFFT_run128Pt;
// Step 2: Initialize the handle
handleCFFT = &CFFT;
// Step 3: Calling the init() will setup the twiddle factor table
// and run the Forward FFT followed by an unpacking routine
CFFT.init(handleCFFT);
CFFT.run(handleCFFT);
CFFT_unpack(handleCFFT);
This project didnt have inverse FFT in it so we've included it performing following steps:
// Step 1: Switch the input and output pointers of the CFFT object
pTemp = CFFT.pInBuffer;
CFFT.pInBuffer = CFFT.pOutBuffer;
CFFT.pOutBuffer = pTemp;
// Step 2: Assign the IFFT function to the run pointer
CFFT.run = (void (*)(void *))ICFFT_run128Pt;
// Step 3: Run the routine
CFFT_pack(handleCFFT);
CFFT.run(handleCFFT);
CFFT_conjugate(handleCFFT->pOutBuffer, handleCFFT->nSamples);
we have performed forward and inverse FFT within same example.
Input array provided is of 256 points.
Output obtained after inverse FFT is not the same as input.
Input(for forward FFT) and Output(from ICFFT_run128Pt) array are plotted and shown below:
Input: (+/- 4096 Vpk)
Output: (+/- 1000 Vpk) with distortion.
The output from ICFFT_run128Pt is distorted as well as scaled down by a factor of 4.
Is there any solution for this problem?
Guide us if we are doing wrong.
Regards,
Shashank.