Part Number: TMS320F28377S
Hello TI Community,
I am currently trying to flash onto the TMS320F28377S. I am using a XDS100v2 JTAG emulator. CCS detects verifies the connection as successful. I am able to flash my program onto the LaunchXL-F28377S board no problem as well. When I try to debug my actual project I get the follow error:
C28xx_CPU1: GEL Output: Memory Map Initialization Complete C28xx_CPU1: Error: (Error -1135 @ 0xC0CC) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.579.0) C28xx_CPU1: Trouble Halting Target CPU: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.579.0) C28xx_CPU1: Error: (Error -1135 @ 0xC0CC) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.579.0) C28xx_CPU1: Unable to determine target status after 20 attempts C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x00130@Program: target is not connected C28xx_CPU1: Error writing the PLL values. (Flash algorithm returned error code). Operation cancelled. C28xx_CPU1: File Loader: Memory write failed: Unknown error C28xx_CPU1: GEL: File: C:\Users\brenden.fung\Desktop\Spectro Rev. B\SPECTRO_B - Project Workspace\EIS_Drive_Utility_REV_B_EVAL_BOARD\Debug\EIS_Drive_Utility_REV_B_EVAL_BOARD.out: Load failed. C28xx_CPU1: Error occurred during flash operation: Could not read register PC: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F800@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005FC00@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected C28xx_CPU1: Error occurred during flash operation: Could not read 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_en.alg C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled. C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D22E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D222@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D214@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected C28xx_CPU1: Error occurred during flash operation: Could not read 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_dis.alg C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled. C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write register PC: target is not connected
I am not sure what the issue is. I recently replaced the TMS320F28377S onto my project and I am testing it for the first time. In the past one of my project partners were able to flash the blinky project onto the chip using the JTAG connector and apparently it worked so I am not sure what the issue is.