Hi, this is the module diagram of ADC-A, it seems that only ADCINA0-5 are connected to a specific pin of the device. so how about ADC6,7,10,11?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, this is the module diagram of ADC-A, it seems that only ADCINA0-5 are connected to a specific pin of the device. so how about ADC6,7,10,11?
Thanks.
Devin,
so how can i find the specific pin for ADCINA6 of such as F28379D? Neither datasheet nor technical reference manual can i find such information.
Hi Howard,
Yes, these MUX settings can't be used and shouldn't be used.
This isn't any different than previous C2000 devices where not all 16 ADC inputs were pinned out.
The general architecture of up to 4 ADCs with 16 channels each would allow us to use the same architecture to build a device with up to 64 internal and/or external channels, but the largest device to date doesn't use nearly that many. This table in the datasheet specifies how many external pins are available: