Part Number: F28M35H52C
Hello, I struggle with the M3 DCSM unlock sequence...
What I would like to do is reset the security to a clean state with CSM-ARMED (bit-11) being set.
I try to get to this state by first setting the FORCESEC bit, and then performing a dummy read to the password locations. This seems to work when performed using the JTAG emulator, but when I run the same sequence from non-secure RAM in the MCU, I cannot get the CSM to arm. Below is the test code and debug output. I must be missing something fundamental.
Debug terminal:
CSM status before forcesec: 0x00001F80 CSM status after forcesec: 0x00000460 OTPSECLOCK: 0x00FFFFFF CSM status after OTPSECLOCK read : 0x00000460 CSM status after password read : 0x00000440
Code:
volatile unsigned long status, temp;
// disable Protection
HWREG(SYSCTL_MWRALLOW) = 0xA5A5A5A5;
status = HWREG(CSM_BASE + DCSM_O_Z1_CR);
DEBUG_WRITE_STRING("CSM status before forcesec: 0x");
DEBUG_WRITE_LONG(status);
DEBUG_WRITE_STRING("\n\r");
// start clean
HWREG(CSM_BASE + DCSM_O_Z1_CR) |= DCSM_CR_FORCESEC; // FORCESEC = 1
status = HWREG(CSM_BASE + DCSM_O_Z1_CR);
DEBUG_WRITE_STRING("CSM status after forcesec: 0x");
DEBUG_WRITE_LONG(status);
DEBUG_WRITE_STRING("\n\r");
status = HWREG(0x680800); // OTPSECLOCK in OPT
status = HWREG(CSM_BASE + 0x120); // OTPSECLOCK register
DEBUG_WRITE_STRING("OTPSECLOCK: 0x");
DEBUG_WRITE_LONG(status);
DEBUG_WRITE_STRING("\n\r");
status = HWREG(CSM_BASE + DCSM_O_Z1_CR);
DEBUG_WRITE_STRING("CSM status after OTPSECLOCK read : 0x");
DEBUG_WRITE_LONG(status);
DEBUG_WRITE_STRING("\n\r");
temp = HWREG(FLASH_BASE + ZONE1_CSMPSWD0_OFFSET);
temp = HWREG(FLASH_BASE + ZONE1_CSMPSWD1_OFFSET);
temp = HWREG(FLASH_BASE + ZONE1_CSMPSWD2_OFFSET);
temp = HWREG(FLASH_BASE + ZONE1_CSMPSWD3_OFFSET);
status = HWREG(CSM_BASE + DCSM_O_Z1_CR);
DEBUG_WRITE_STRING("CSM status after password read : 0x");
DEBUG_WRITE_LONG(status);
DEBUG_WRITE_STRING("\n\r");