This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28374D: max Perx.sysclk for peripherals like UART . SPI etc

Part Number: TMS320F28374D

Hello everybody , 

please to have minimum baudrate error   in  my UART , I would like to use  max persysclk of 200MHz  for Uart system clock  :  do you see any issue ?

I can see on figure 2-153   register LOSPCP can be set accordingly ( no prescaler  ) , and I do not see any limititation in DS , but I would like to be confirmed on this .this clock is used also by SPI , SCI and MCBSP .

on top can I do something similar in F28065 ? so have  0 prescaler also there ?

thank you very much

bye

Carlo