Part Number: TMS320F28035
Does these CLA registers can be write by the CPU?
//__meallow();
//Cla1Regs.MICLR.bit.INT1 =1;
//Cla1Regs.MICLROVF.bit.INT1 =1;
//Cla1Regs.MCTL.bit.SOFTRESET =1;
//ClaRegs.MIER.bit.INT =0;
//__medis();
And my customer used a 300K Hz PWM to trigger a CLA task, and the code exectution time of the CLA task may be > (1/300K second) sometimes ,which will result in interrupt overflow, so they want clear the overflowed interrupt(they try to use the register as mentioned earlier,but have no effect).Does anyone have a solution of this question? They should not change the pwm frequency.
Thanking you!