Part Number: TMS320F28377S
Other Parts Discussed in Thread: ADS6125
In TMS320 series there are both microcontrollers and DSPs.
It is said:" If the digital lock-in amplifiers have access to the processing power of a DSP, the multiplication of r(t) and m(t) can be implemented directly in firmware." Is it true to TMS320 series? Dose TMS32028377S work well to implement this kind of multiplication? In low frequency range digital lock-in amplifiers are popular, below 2MHz, but higher frequency range, for example, over 10MHz.