Part Number: TMS320F28027
Other Parts Discussed in Thread: CONTROLSUITE, LAUNCHXL-F28027,
Tool/software: Code Composer Studio
Hi all,
I am trying to flash program TI 28027 using Black Hawk USB2000 controller. The TMS 28027 was soldered onto a breakout board. The following connections were done
(TRST,TMS,TCK,TDI,TDO,XRS), VDD and VSS. I have not connected external oscillator. The VREG has been grounded. I am using the flash program example available in control suite. However, I am getting the following errror.
C28xx: Failed CPU Reset: (Error -1156 @ 0x6) Device may be operating in low-power mode. Do you want to bring it out of this mode? (Emulation package 6.0.83.0)
I have two queries:
a) what is the reason for this error. Any specific connections that may have been left out.
b)What are the necessary connections to flash program 28027 using Black Hawk USB 2000 controller. Any references for the procedure and connections to be done.
Thanking you