This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TMS320F28335: Unexpected program execution

Part Number: TMS320F28335

Tool/software: TI-RTOS

Hello, 

I am using Flash API V2.10 to execute Flash operations on TMS320F28335. 

I use Flash_CallbackPtr to feed watchdog and to send a CAN message as a keep alive.

This is my callback function:

#pragma CODE_SECTION(Flash_Callback,"ramfuncs");

void Flash_Callback(void)

{

       static Uint16 j= 0;

       byte _p_Data[2]= {1,0};   //Erasing

       EALLOW;

       SysCtrlRegs.WDKEY = 0x55;        /* serve watchdog #1 */

       SysCtrlRegs.WDKEY = 0xAA;        /* and serve watchdog #2 */

       EDIS;

       j++;

       if(j>13900)

       {

             CanSendMessage(0x19D0133A,      0, _p_Data); //in ram

             j= 0;

       }

}

When the program calls to the Flash28335_Erase function the program executes the erasing and the callback (CAN message is sent). After the erasing has finished, the program execution goes I don't know where but it is not halted. After some time, the DSP is restarted.

If I suspend the execution before the restart, I always see this: 

 

Moreover, after some investigations, I could see that declaring p_Data[2] as static solves the problem, the program execution after the erasing is normal. It doesn’t make sense to me and I guess that the real problem if somewhere else. Could you help me?

This is the development environment:

DSP: TMS320DSP28335

Compiler: 6.2.5

XDCTools: 3.30.4.52

SYS/BIOS: 6.41.0.26

CCS: v6.1

Regards,

Paloma