Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
I am using CCSV5 for the first time and want to run the blinky example. When I try to build the project, I got some errors.
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "Blinky.out" not built
the following is the program and console output
//###########################################################################
//
//! \addtogroup f2806x_example_list
//! <h1>Timer based blinking LED(timed_led_blink)</h1>
//!
//! This example configures CPU Timer0 for a 500 msec period, and toggles the GPIO34
//! LED once per interrupt. For testing purposes, this example
//! also increments a counter each time the timer asserts an interrupt.
//!
//! \b Watch \b Variables \n
//! - CpuTimer0.InterruptCount
//!
//! \b External \b Connections \n
//! Monitor the GPIO34 LED blink on (for 500 msec) and off (for 500 msec) on
//! the 2806x control card.
//
//###########################################################################
// $TI Release: F2806x C/C++ Header Files and Peripheral Examples V150 $
// $Release Date: June 16, 2015 $
// $Copyright: Copyright (C) 2011-2015 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
// Prototype statements for functions found within this file.
__interrupt void cpu_timer0_isr(void);
void main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2806x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initalize GPIO:
// This example function is found in the F2806x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2806x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2806x_DefaultIsr.c.
// This function is found in F2806x_PieVect.c.
InitPieVectTable();
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.TINT0 = &cpu_timer0_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
// Step 4. Initialize the Device Peripheral. This function can be
// found in F2806x_CpuTimers.c
InitCpuTimers(); // For this example, only initialize the Cpu Timers
// Configure CPU-Timer 0 to interrupt every 500 milliseconds:
// 80MHz CPU Freq, 50 millisecond Period (in uSeconds)
ConfigCpuTimer(&CpuTimer0, 80, 500000);
// To ensure precise timing, use write-only instructions to write to the entire register. Therefore, if any
// of the configuration bits are changed in ConfigCpuTimer and InitCpuTimers (in F2806x_CpuTimers.h), the
// below settings must also be updated.
CpuTimer0Regs.TCR.all = 0x4001; // Use write-only instruction to set TSS bit = 0
// Step 5. User specific code, enable interrupts:
// Configure GPIO34 as a GPIO output pin
EALLOW;
GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0;
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
EDIS;
// Enable CPU INT1 which is connected to CPU-Timer 0:
IER |= M_INT1;
// Enable TINT0 in the PIE: Group 1 interrupt 7
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;
// Enable global Interrupts and higher priority real-time debug events:
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
// Step 6. IDLE loop. Just sit and loop forever (optional):
for(;;);
}
__interrupt void cpu_timer0_isr(void)
{
CpuTimer0.InterruptCount++;
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1; // Toggle GPIO34 once per 500 milliseconds
// Acknowledge this interrupt to receive more interrupts from group 1
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
//===========================================================================
// No more.
//===========================================================================
build console text
**** Build of configuration Debug for project Blinky ****
C:\ti\ccsv5\utils\bin\gmake -k all
'Building target: Blinky.out'
'Invoking: C2000 Linker'
"C:/ti/ccsv5/tools/compiler/c2000_6.2.0/bin/cl2000" -v28 -ml -mt --cla_support=cla0 --float_support=fpu32 --vcu_support=vcu0 -g --diag_warning=225 --display_error_number --diag_wrap=off -z -m"Blinky.map" --stack_size=0x300 --warn_sections -i"C:/ti/ccsv5/tools/compiler/c2000_6.2.0/lib" -i"C:/ti/controlSUITE/device_support/f2806x/v151/F2806x_headers/source" -i"C:/ti/controlSUITE/device_support/f2806x/v151/F2806x_common/source" -i"C:/ti/ccsv5/tools/compiler/c2000_6.2.0/include" --reread_libs --display_error_number --diag_wrap=off --rom_model -o "Blinky.out" "./Example_2806xLEDBlink.obj" -l"libc.a" "../28069_RAM_lnk.cmd"
<Linking>
undefined first referenced
symbol in file
--------- ----------------
_ConfigCpuTimer ./Example_2806xLEDBlink.obj
_CpuTimer0 ./Example_2806xLEDBlink.obj
_CpuTimer0Regs ./Example_2806xLEDBlink.obj
_GpioCtrlRegs ./Example_2806xLEDBlink.obj
_GpioDataRegs ./Example_2806xLEDBlink.obj
_InitCpuTimers ./Example_2806xLEDBlink.obj
_InitPieCtrl ./Example_2806xLEDBlink.obj
_InitPieVectTable ./Example_2806xLEDBlink.obj
_InitSysCtrl ./Example_2806xLEDBlink.obj
_PieCtrlRegs ./Example_2806xLEDBlink.obj
_PieVectTable ./Example_2806xLEDBlink.obj
>> Compilation failure
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "Blinky.out" not built
gmake: *** [Blinky.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****