Hi
I am using HVMotorCtrl+PFC kit.
According to the Level 3 Incremental Build, the incremental encoder connected to [Main]-H1 is employed to find the speed/theta of the motor.
According to the Level 6 Incremental Build, SPI interface [Main]-H2 is employed to get the position of the rotor.
I am wondering if I can used both input (H1 and H2) and read from it where my application have two sensors ( encoder for the PM machine and the position of slid ). I would like to use H1 for commutation and speed control and H2 for position control.
Can I use both inputs ?
Thanks