This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-TMDSPLCKIT-V3: TMDSPLCKIR-V3

Part Number: TIDM-TMDSPLCKIT-V3

I am working on the C2000 tmdsplckit-v3 PLC kit. I have set it up correctly according to the guidelines in the start up guide. I have been able to run the PHY test successfully confirming that the two components recolonize each other, but every time I try to send a message I get the error COM6: The message was not delivered. Also My long address for both components is 0000:0000:0000:0000. Is this related to my problem and how should I go about fixing it?

Waiting for Reply,

Thank you.

  • hi Scott,

    There is a new hardware revision for the C2000 tmdsplckit-v3 PLC kit , TMDSPLCKITV4-CEN link below :

     

    The issue "I get the error COM6: The message was not delivered." could be because the device is not set for the correct Diag port & data port .

    The long address can be set using the " Set  G3 configuration " command .

    please check the documentation on Zero config gui in the SDK below .

    regards.