This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-PLC-PLCLITE: PLC Lite Device Mode

Part Number: TI-PLC-PLCLITE


In the PLC Lite host message specification, under section 2.2.3 (LOAD SYSTEM CONFIG), the "Device Mode" value options are 3 and 5.  The former, 3 (P to P) is highlighted in Green.  Is this the required mode for PLC Lite EVEN if more than two nodes will be on the PLC lite network?