Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hello All,
I am working on a project of single phase solar inverter. I need to generate sine pwm for mosfet's gate switches. I have TMS320F28335 microcontroller card along with with experimental kit docking -station .To get sine pwm, i have to do comparison of sine function(50Hz) with a triangular carrier function (20KHz) at the same x-axis reference. Whenever sine function will be greater than triangular function then output should be high other wise it should be low.
I do not know much about c programming. I also do not know how to start writing the code for spwm in C for tms320f28335.
Does above microcontroller card provide sine pwm example codes.
Can some body help me to generate sine pwm. i will be very thank full