Part Number: TMS320F28034
Dear my friends,
I want to get HFI lib ,and use it to develop TMS320F28034, could you tell how could i get it? and Can I get it ? if yes, where?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28034
Dear my friends,
I want to get HFI lib ,and use it to develop TMS320F28034, could you tell how could i get it? and Can I get it ? if yes, where?
Stephen,
I see you sent me a direct message as well, so I will answer you back there.
but in the release notes for
HVPM_Enhanced_Sensorless.c
* BUILD LEVEL 7 *
* ============= *
* The executable for enhanced SMO is in esmo.lib file, which is part of *
* the control suite. The user is free to evaluate the function of esmo *
* using this executable. For access to its executable code, the user is *
* advised to contact the nearest TI sales office or distributor. *
* *
* BUILD LEVEL 8/9 *
* =============== *
* The executable for Initial Position Detection (IPD) and *
* High Frequency Injection (HFI) are in hfi.lib file, which are not *
* part of the downloadable version of control suite. *
* Any attempt to build LEVEL8/9 code will result in error. *
* For access to the library and/or executable code, the user is advised *
* to contact the nearest TI sales office or distributor. *
basically for HFI.lib sales must request from us directly. We don't release it unless there is a business case.