Other Parts Discussed in Thread: TMS320F28027, LAUNCHXL-F28027, CONTROLSUITE
Hello,
This may be a straightforward question, but I was wondering what the difference between TMS320F28027F and TMS320F28027 ?
I have flash locked my device and I would like to replace the IC on the Launchpad. I understand that buying the LAUNCHXL-F28027F will be easier but I have already proceeded to solder the pin outs to other connections and it has been locked to place. So, changing out the whole controller is not an option.
I was not able to find the hardware package for the LAUNCHXL-F28027F with the bill of materials to know which MCU is installed on it. I was able to find the hardware package of LAUNCHXL-F28027, which pointed that TMS320F28027PTS is installed on it.
I checked under the microscope and saw that LAUNCHXL-F28027F has TMS320F28027PTT installed.
My question remains now is that the only difference between the two is that:
1. TMS320F28027PTT - Has INSTAspin
TMS320F28027PTS - Does not have INSTAspin
is this information correct?
2. Where can i find the hardware package for LAUNCHXL-F28027F ?