Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Tool/software: Code Composer Studio
I am tring to generate ePWM3 pulse to trigger ADC sampling with the following config
EPwm3Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm3Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from CMPA on upcount
EPwm3Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm3Regs.CMPA.half.CMPA = 0x0080; // Set compare A value
EPwm3Regs.TBPRD = 0xAFC8; //TBCLK=SYSCLK/(HSPCLKDIV*CLKDIV)=45MHz this gives 1KHz pulse
EPwm3Regs.TBCTL.bit.CTRMODE = 0; // count up and start
but ADC is not triggered, I also config GPIO04 to observed if ePWM3A, no pulse seen
GpioCtrlRegs.GPAPUD.bit.GPIO4 = 0; // Enable pullup on GPIO4
GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // 0=GPIO, 1=EPWM3A, 2=Resv, 3=Resv
I have checked the epwm3 clock is enabled.
Can anyone see what causes the problem?