Other Parts Discussed in Thread: C2000WARE
Hi all,
Working on standalone application, the requirement will be an application on PC side which will trigger the SCI boot,
need to impliment a F28379 bootloader code to support SCI boot using Launchpad, Is it possible using con1, the schematis attached.
Please can anybody give some starting points from where to start?
Myself worked worked on some examples code like adc demo and blinking leds using the CCSV7 and C2000ware.
Also find some SCI boot code in the below directory path and SCI BOOT method called in the c1brom_boot.c file.
ti/C2000Ware_1_00_01_00/libraries/boot_rom/f2837xd/revB/rom_sources/F2837x_bootROM/cpu01-bootROM/source/SCI_Boot.c
Is there any example project readily available on C2000 ware, please provide me any inputs.