This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F28069M: BLDC- Commutation Signls (UVW) - Motor Control

Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: MOTORWARE, CONTROLSUITE, INSTASPIN-BLDC

Tool/software: Code Composer Studio

Hi,

I have application where I generate BLDC commutation signals (UVW) using an external sensor chip and I need to control the motor based on those signals generated by reading those signals to some GPIO's on the controller board. Is there a lab in the Insta-spin example projects that actually does the job or do i need to write a program from scratch. I am using DRV-8301 EVM Rev D board with 28069  control card. Any help is really appreciated.

Thank you,

Bhanu.  

  • If you are using an F28069F or F28069M device, you can use InstaSPIN-FOC to control the motor. Please find all relevant examples in our Motorware download.

    If your device does not have an 'F' or 'M' suffix, you can use our older InstaSPIN-BLDC examples in ControlSUITE.

    Sean