hello
I am having problems regarding interfacing of f28027 with analog signals (current, voltage). I am programming my device with Simulink by using hardware support and my processor needs input from circuit to implement closed loop control which is current and voltage. Currently, I am using hall effect current sensor acs712 and voltage divider but they are not working. I also need to know which data type is selected from unint8, single, double, unint32 for ADC pins to enable them to read the data.